F3SG_SRA Sample Code.SMC2:
Sample code using the IAG's and function blocks using a NX1P2 and EtherCat Coupler and an NX-ILM400 I/O Link module. Currently the IAG's are set up to use with a NA 12 or 15 inch screen. This is the same sample code as in the function block documentation.


Omron_F3SG_SR_7_9.iag:
Created IAG library file for a 7" and 9" NA that can be loaded into a project and used.


Omron_F3SG_SR_7_9.SMC2:
IAG source code  for a 7" and 9" NA that can be used to modify the IAG's if needed.


Omron_F3SG_SR_12_15.iag:
Created IAG library file for a 12" and 15" NA that can be loaded into a project and used.


Omron_F3SG_SR_12_15.SMC2:
IAG source code  for a 12" and 15" NA that can be used to modify the IAG's if needed.


TechNote_SLC_0001.0_F3SG_SRA_IAG's.PDF:
Tech note showing how to use the IAG in a project.